STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

STM32WL55JC1 is not sending or receiving

Hello everyone, I am using 3 STM32WL55JC1. One for base station and the other two's for sensor node. Everything was fine but then I started UART communication between base station and ESP32. I started coding ESP32 so I unplug the usb cables of stm32w...

AHakk.1 by Associate III
  • 4596 Views
  • 9 replies
  • 0 kudos

BLE Data Throughput Issue - STM32WB5MMGH

Hi,I have been using STM32WB5MMGH for transmitting PCM Data. I used BLE data throughput method from the example code for transmitting data. Audio sample rate is 8000 Hz, that 8000 data is transmitted in a buffer size of 244. The sample is of 16-bit i...

LR.2 by Associate III
  • 1190 Views
  • 0 replies
  • 0 kudos

I-NUCLEO-LRWAN1 wrong APPEUI

I just bought a LRWAN2 pack, I was able to connect the gateway to the TTN network and application server. But the APPEUI i the join request was wrong (only zeroes). So I plugged an oscilloscope on the RX and TX pins an it shows that:Does this mean th...

_legacyfs_online_stmicro_images_0693W00000dDdTxQAK.png
YLebo.1 by Associate
  • 1500 Views
  • 1 replies
  • 0 kudos

STM32WB BLE packet missing and INSUFFICIENT_RESOURCES

Hello all,We are using BLE to send packet of 23 bytes every 5 ms. Since we have noticed that some packets are lost, we are trying to investigate to understand what's happened. In addition to lost packets, for almost every packet, we get the error BLE...

audrey38 by Associate II
  • 4239 Views
  • 5 replies
  • 0 kudos

Issue in upgrading BLE stack using CLI

When I tried to upgrade the BLE stack(v1.16.0) for the first time then am able ti upgrade it properly.Then I tried to upgrade it again it showed me the following error. 

Mkuma7_0-1692351615085.png
Mkuma.7 by Associate III
  • 843 Views
  • 0 replies
  • 0 kudos