STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STEVAL-L99615C wireless communication

Hi All!I have some doubts about possible connection STEVAL-L99615C with for example X-Nucleo-IDB05A1. As far as I understand it should works, but I am not sure if it will be possible to get data send by bluetooth to computer and then read them in ded...

jojoanaa by Associate
  • 947 Views
  • 0 replies
  • 0 kudos

Probe lines in STM32CubeWL FW (LoraWAN)

Hi there,I am wondering what the probe line settings in the LoraWan software pack are for (End node skeleton).My guess is they are used to signal the occurance of some events while SWD debugging is disabled, but I couldn't find any usage of them in t...

STM32WB fus not starting

Hi.I have nucleo board with STM32WB55RGV6 mcu. Trying to start FUS using StCubeProgrammer (swd mode), and unable to start it and even get its version. I do what is described in wiki: connect in normal mode + hardware reset, start fus, disconnect, sta...

Screenshot 2023-09-20 at 10.57.30.png

Resolved! NUCLEO-WL55JC1 for instant digital audio transmission

HelloI want to build an In-Ear Monitor system for performing music live. This system gets an audio signal from a sound card. Transmits it wirelessly (around 865MHz) to a bodypack receiver and plays the audio with virtually no delay.I stumbled upon th...

Kenney by Associate
  • 2431 Views
  • 2 replies
  • 0 kudos

STMicroElectronics Partnership with Espressif

Is STMicroelectronics ever going to partner with Espressif to integrate short distance wireless connectivity with stm32 MCUs? Would this be a good idea? Right now, the only good library that integrates Wi-Fi connectivity and networking in stm32 using...

Tizio1234 by Associate II
  • 1268 Views
  • 0 replies
  • 0 kudos

ZigBee timeout to join the network

Hi,The ZigBee Coordinator does not allow the new nodes to join the network after a certain amount of time. I want to change this behavior. I want the coordinator allow the new nodes to join the network at any moment of work. How to change it?Best Re...

lukasz2 by Associate III
  • 6038 Views
  • 3 replies
  • 0 kudos

Is periodic advertising sync supported by the coprocessor?

I'm trying to enable periodic sync so that another BLE device can sync with the stm32wb5mmg and receive advertising data from it. Through bluetooth sniffer I can see that the 'Sync Info' flag in the Extended Header Flags is set to zero, meaning no sy...

ADing.1 by Associate II
  • 1074 Views
  • 0 replies
  • 0 kudos

STM32 LOCKUP causes in the field?

We're using the STM32WB55CE across a range of products, using a mostly shared codebase. Thousands of devices deployed and mostly very stable, but one particular device (the one with the largest code base) is causing a lot of grief..After a few weeks ...

ChrisLB by Associate III
  • 1894 Views
  • 1 replies
  • 0 kudos