STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

STM32WB CPU2 reset

Hello, how can I call a full reset of the CPU2/BLE stack (as if the device were powered up)?I'm resetting CPU1, which then restarts the CPU2/BLE stack from some other code. But this causes some corruption with BLE notifications.

MHast.1 by Associate II
  • 1842 Views
  • 1 replies
  • 0 kudos

Cannot debug M0+ STM32WL55 in SBSFU Dual core project

Hi everyone, I try to debug CM0+ core (using GDB server) application LoRaWAN in SBSFU dual core project. If I only run the debugger on CM4, the program will start and run normally. But when I try to debug CM0+, it will not run and my program failed.I...

STM32WL how to enable RTC subsecond underflow interrupt

STM32WL lorawan middleware use a RTC subsecond underflow interrupt update tick instead systick,but the subsecond underflow interrupt never entered.It seems interrupt not enabled, so I manually enable RTC subsecond underflow interrupt but the handler ...

SimonLaw by Associate
  • 1828 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL55 LoraWan End Node and SubGhz_Phy comunication

Good morning,I am creating an application that would require the use of several stm32wl55.The idea is to have one microcontroller configured as a LoraWan EndNode communicating with TTN and a set of Slaves communicating via subghz (which will be slave...

IngSerio by Associate III
  • 6943 Views
  • 5 replies
  • 1 kudos

How to send data by STM32WB BLE Server?

In the STM32WB Workshop video I can understand how to send data and control the LED but how to read data is not explained. I want to read data from STM32WB BLE. Can you someone help me in regards to this?

Resolved! sigfox credentials.zip problem

Hey guys. I'm trying to collect the sigfox credentials through the website https://my.st.com/sfxp and once the download is done,the file is corrupted and I can't extract it.How can I solve this problem? 

mmachadopereira_0-1696741872387.png

Resolved! STM32WLE5CC HSE32 TCXO input

Greetings!I'm designing a board using STM32WLE5CCU6 MCU and decided to use a 32-MHz Clipped Sine Wave TCXO instead of a crystal for the HSE32 clock.I have a question regarding the additional circuitry between the TCXO and MCU, is an AC coupling capac...

DTomi.1 by Senior
  • 7755 Views
  • 5 replies
  • 0 kudos