STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB5MM-DK, connecting to Tuya gateway with zigbee

Hello,How should I make connection to the Tuya gateway with zigbee? I have read zigbee wiki dokumentation about zigbee binding. I have understand that I should use "find and bind" mechanism in that case. I tried to find suitable example from github, ...

eskomj by Associate III
  • 12187 Views
  • 12 replies
  • 0 kudos

Resolved! STM32WB55RG USB Device Not Recognize by Comp

Hi,I'm trying to use usb device of my STM32WB55RG Nucleo board but when I connect my device to computer, I got a "USB Device not recognized" error. I used "LL_HSEM_1StepLock( HSEM, 5 )" function before APPE init. How can i get rid of this error?Best ...

Wireless M-Bus (wMbus) and LoRaWAN

Hello,We are in the process of developing a smart meter that will feature dual communication capabilities supporting both Wireless M-Bus (wMbus) and LoRaWAN. Our aim is to use a single chip for this purpose, with the advantage of sharing the same ant...

Resolved! STM32WB How to use GATT caching?

Hello,I'm using BLE_p2pClient and BLE_p2pServer programs.I had pairing request in BLE_p2pClient to have both devices bonded.Now, I want to have a fast connection between client and server; actually, the connection between client and server is about 2...

FWX by Associate III
  • 3146 Views
  • 5 replies
  • 0 kudos

Resolved! X-CUBE-BLE1 SampleApp: How it works ?

Hi ST Community,I'm using the B-L475E-IOT01 card and I want to use the X-CUBE-BLE1 middleware to send information directly to a variable (something I was thinking of doing simply with this application). Only, when I run it and try to debug, I'm havin...

FUS running but not able to load Stack?

I am trying to load the p2p server example and noticed my Nucleo-WB15CC doesn't do any bluetooth communication. I can run normal user code just fine (LEDs, GPIO etc.) but CPU2 doesn't seem to do anything.When I try to start FUS, I get this:When I try...

tester_1-1691183454986.png tester_0-1691183405200.png
tester by Associate III
  • 5377 Views
  • 8 replies
  • 0 kudos