STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 227 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4070 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL55 no rf

Good dayI am using the STM32WL55 chip for a project. I did preliminary tests using the NUCLEO-WL55JC2 Development board.I created a custom PCB following the design of the Development board.When I program the custom board with the same firmware that w...

SDu T by Associate III
  • 1968 Views
  • 2 replies
  • 0 kudos

STM32WB55: C2 randomly enters spin loop

I find that when entering deep sleep/range 2 using aci_gap_set_non_discoverable(), C2 would not reliably enter the ultra low  (~4uA) power consumption mode, current would jump to ~5mA. I am using stack 1.18 and even 1.19.  a) Calling aci_gap_set_non_...

rudivs by Associate
  • 1398 Views
  • 1 replies
  • 0 kudos

Resolved! SPI: changing CPOL between transmissions

I have 2 devices on my SPI bus that need different CPOL settings. both use CPHA = 0 and the SPI peripheral is configured to use Motorola frame format.Communication works with both devices if their respective CPOL setting is set in CubeMX (and thus fi...

connoisseur_de_mimi_1-1715784526043.png connoisseur_de_mimi_2-1715784647618.png connoisseur_de_mimi_3-1715784945416.png

Unable to update FUS or flash the wireless stack STM32WB55

H,I just had some custom boards with STM32WB55CG and I would like to flash the BLE stack into the microcontroller. For some reason the STM32CubeProgrammer does not allow me to flash the FUS or BLE stack files, it always comes back with warning/errors...

ALu.3 by Associate II
  • 9807 Views
  • 9 replies
  • 0 kudos

NUCLEO WB55RG BLE Periferal can not paring

I am developing a BLE peripheral device using the NUCLEO WB55RG. I am having trouble connecting to smartphones. The pairing process is as follows: The security is Just Work, using bonding mode.During the first pairing:The peripheral sends a security ...

Problem with third party library integration

I am trying to include a tinycbor .h file and as per third party include method i have done all the step but still i get the error about the linker didn't find a definition of library API functions. Here is the all the screenshot of my project and lo...

Hardik02_0-1710890786632.png Hardik02_1-1710890912531.png Hardik02_2-1710891033500.png Hardik02_3-1710891126664.png
Hardik02 by Associate II
  • 1452 Views
  • 1 replies
  • 0 kudos

ST ble sensor no device founded

Hi allI'm new on stm32 ble applications.Starting from st example BLE_OTA I developed my custom bootloader for my STM32WB55 nucleo board.I encountered the following issues:1) St ble sensor mobile app (from play store) can't detect my device; I compile...

kappa182 by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos