STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB5MM OTA Application at a different address

I have multiple questions:1. Is there a limit on the firmware size in STM32WB series? If yes, what is the limit?2. Is there a limit on the firmware size of the OTA application in STM32WB series? If yes, what is the limit?3. I want to perform OTA at a...

Lalit1 by Associate
  • 1190 Views
  • 1 replies
  • 0 kudos

STM32WL5 2nd core reset

Hi,I'm using STM32WL5 SoC in my lora project.I started from this example: "LoRaWAN_End_Node_DualCoreFreeRTOS".In my board, I have a problem at startup, CPU2 doesn't start after a simple pin reset (NRST).The only way is to switch power supply off, wai...

DiegoKer by Associate
  • 1111 Views
  • 1 replies
  • 0 kudos

BLE Connection issue on p2p Client

Hello all,         In my project I'm using STM32WB5MMG MCU for BLE Server and Client.BLE Connection between p2p Server and p2p Client is working well but I want connect Custom Templete Server with p2p Client.In this case Server and Client are not con...

WhatsApp Image 2024-04-25 at 3.41.54 PM.jpeg WhatsApp Image 2024-04-25 at 3.14.00 PM.jpeg
Kavinraj by Associate III
  • 1219 Views
  • 1 replies
  • 0 kudos

How to factory reset ASTRA1B

Hi,Bought online  ASTRA1B  previously used,  for school project,I do not have experience with  ST Boards.Need Help with following:where to find stock firmware (default factory firmware)  ?Do I need STLINK-V3MINIE for flashing firmware ?How to factory...

Resolved! Costum board stuck at PeriphCommonClock_Config();

hi, Im using my own costum board with a STM32WBA52CG on it. When I'm nog using the RF my code is working perfectly. When I activate the RF in the STM32CubeIDE, my code is stuck in  PeriphCommonClock_Config();More specifically in the following code: I...

Screenshot 2024-05-07 at 17.34.13.png
matsmort by Associate II
  • 2532 Views
  • 4 replies
  • 0 kudos

HCI_COMMAND_COMPLETE_EVT_CODE cannot be received

BLE peripherals are implemented using NUCLEOWB55RG.I would like to check if Advertsing is working properly by receiving the completion of the asynchronous aci_gap_set_discoverable execution with HCI_COMMAND_COMPLETE_EVT_CODE, HCI_COMMAND_COMPLETE_EVT...

STM32WL DAC Sample-And-Hold: Internal capacitor?

I want to generate a constant, steady voltage as COMP INPM in STOP1 with the DAC (using HAL libs at the moment).Unfortunately I cannot get a steady signal. The voltage drifts around some seconds, stabilises and starts from the beginning (oddly seems ...

surumadurum_0-1713209445540.png

SIGFOX_API_start_continuous_transmission

Using this API returns 0x3157 error code after running SIGFOX_API_close successfully (return code is 0), anyone tried that? What are we missing here?BTW - Same behavior observed when using ST provided Sigfox_AT_Slave_DualCore example out of the box w...

ASchw.1 by Associate II
  • 2204 Views
  • 4 replies
  • 0 kudos