2024-05-04 12:41 AM - edited 2024-05-04 1:37 AM
Hi,
Bought online ASTRA1B previously used, for school project,
I do not have experience with ST Boards.
Need Help with following:
where to find stock firmware (default factory firmware) ?
Do I need STLINK-V3MINIE for flashing firmware ?
How to factory reset ASRTA1B ?
If ASTRA1B can be reflashed usigng USB C, Please provide steps or link document where these steps are mentioned.
Observed "Time Out" messages in console, dont know if this is due to hardware fault or firmware ?
VERB URC:152s556:IRQ_RX_TX_TIMEOUT SHOW NEW LoRa KEYS VERB URC:166s687:MAC txDone VERB URC:171s720:RX_1 on freq 868300000 Hz at DR 0 VERB URC:171s918:IRQ_RX_TX_TIMEOUT VERB URC:171s918:MAC rxTimeOut VERB URC:172s720:RX_2 on freq 869525000 Hz at DR 0 VERB URC:172s918:IRQ_RX_TX_TIMEOUT VERB URC:172s918:MAC rxTimeOut
|
Thank You
Suds
2024-06-02 10:14 AM
Hello @technofreaks
I suggest you to follow the UM2966. It should guide you on the best way to use this evaluation kit.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.