STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB CPU2 hard fault in HCI stack variants in v1.20.0

Hello!I'm trying to update from v1.11.0 to the latest stack in our firmware for stm32wb5x_BLE_HCILayer_fw.bin to address the errata around the utilizing the PLL, but CPU2 is hard faulting as soon as we invoke SHCI_C2_BLE_Init(...).I can run and load ...

Tim.N by Associate III
  • 3271 Views
  • 6 replies
  • 1 kudos

Resolved! Zigbee Traces No Output

Hello,I am trying to get zigbee traces running on STM32WB5MMG running on Sparkfuns development boards.For my current project I am using this hardware:SprakFun MicroMod Main Board - Single - https://www.sparkfun.com/products/20748SparkFun MicroMod STM...

Name by Associate III
  • 1975 Views
  • 2 replies
  • 0 kudos

Anti-Rollback feature

I need to express my frustration with this feature. For some reason, I accidentally activated the anti-rollback feature. Now, when I try to update the new firmware, I am unable to write a new one. As a result, it's completely bricked for any future w...

Resolved! LoRWAN for STM32F4

Hi all,i am new to the STM MCU and i am working on project about LoRaWANi have a ST32F401 MCUall the sources and examples i found about LoRaWAN supports different modells.so i wanted to ask if theres any sources or examples that support the modell i ...

ward by Associate II
  • 1132 Views
  • 1 replies
  • 1 kudos

Resolved! The STM32WB can not STOP or Sleep?

Hi,we are using the STM32WB microcontroller along with sleep modes – specifically, SLEEP and STOP2. When we try to enter STOP2 (or Sleep) mode, it seems like the MCU automatically checks whether it can enter this mode or not (like an automatic check ...

JR2963 by Senior II
  • 1588 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55CG Zigbee connection Tuya Smartlife

Hi together,I have the STM32WB55CG and plan to integrate it into a smart home Zigbee network, that uses the Tuya Gateway and is controlled by Smartlife app.I have found several examples on how they communicate with each other (network of STMs), howev...

vh789 by Associate III
  • 2038 Views
  • 3 replies
  • 2 kudos

STM32WLE5CC join accept not seen

I'm using a STM32WLE5cc inside a RAK3172 (TCXO) module on a custom board. I have custom firmware developed in the STMCube IDE. So, my join request is seen on the gateway, and the gateway sees a join accept from the server. Unfortunately the joined ev...

SLevi.1 by Senior
  • 1798 Views
  • 2 replies
  • 0 kudos