STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 138 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4033 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 Ble Configuration

Hi, I am using the STM32WB55CCU6 base custom board. In that board i am not using LSE crystal oscillator (32.768Khz). Is it possible if i can run my BLE application without the LSE?Please provide your suggestion in as soon as possible. Thanks in advan...

ksaini by Associate
  • 1074 Views
  • 1 replies
  • 0 kudos

BLE Operation in Low Power Modes on STM32WB

Hi,I'm not sure if I fully understand how the low-power mode works with active BLE on the STM32WB. I have an application using FreeRTOS and the BLE stack. I have set up advertising and am able to send and receive data over BLE. This works fine. When ...

JR2963_0-1726493511723.png
JR2963 by Senior II
  • 2349 Views
  • 3 replies
  • 0 kudos

BLE keep connection alive

What is the proper way of keeping connection from Client to Server alive?I'm working with smart glasses and after connection STM32 client sends the data, however, after some 10-20 seconds or so glasses show "Client disconnected" message.What puzzles ...

roman_tl by Associate II
  • 2305 Views
  • 2 replies
  • 0 kudos

Decoder for LoRa messages for Datacake

Hello, I followed the indtructions from here, https://www.youtube.com/watch?v=vuc6914B0KM and I setup the NUCLEO-WL55JC STM32WL Nucleo-64 board and sensor board X-NUCLEO-IKS01A3 with LoRaWAN Gateway P-NUCLEO-LRWAN2 through The Things Network (TTN). I...

MihaiMEC by Associate
  • 1472 Views
  • 1 replies
  • 0 kudos

Resolved! Zigbee and BLE at once on STM32wb5mm-dk

I have two stm32wb5mmdk which I tried to create a custom BLE MESH but failed miserably . I am trying to use zig-bee to send data from one to other , and then transfer the same data to a mobile phone using BLE.Is there an example or MOOC available for...

Rituraj by Senior
  • 1430 Views
  • 3 replies
  • 0 kudos