cancel
Showing results for 
Search instead for 
Did you mean: 

stm32wl5 discontiguous ram, accessing ram2

STMGuitartune68
Associate II

I am currently working with a stm32wl55JCI and using RTOS. I am currently running into overflow errors of ram1. I am currently using an example project using RTOS. I tried using heap5 and used the sample templates for how to define the memory regions but It did not allow for memory access. Is there a procedure that must happen for accessing ram2? Is there a specific function I must use from the HAL library or anything I have to enable through the ioc? 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0