STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! SHCI_C2_BLE_Init Never Returns in BLE_Ota

I have a custom board which is based heavily on the P-NUCLEO-WB55.Nucleo.  If I flash my board with a slightly modified version of BLE_Ota it will appear in ST BLE Sensor, at which point I can use it to flash my application.  This works.  After flash...

Screenshot_20240926_133052_ST BLE Sensor.jpg Jcoll1_3-1727372047380.png Jcoll1_0-1727373323388.png
Jcoll.1 by Associate III
  • 1895 Views
  • 3 replies
  • 0 kudos

Resolved! P-NUCLEO-WB55 USB Dongle

Hello everyone,I am looking for a USB Bluetooth/Zigbee module like the WB55CG USB dongle that is part of the P-NUCLEO-WB55.Can anyone tell me if the module is also available as a standalone product?If this is possible, can someone answer the followin...

Edmund by Associate II
  • 1472 Views
  • 1 replies
  • 1 kudos

Resolved! Sending LoRa packet takes more than 1.5 sec.

Hi guys,I'm playing with STM32WL (the Nucleo-STM32WL55JC1 to be precise). Also I'm using the SX1303 LoRa gateway (it's a RPi Hat from Waveshare).Node is next to the gateway.When it comes to send of the data, it takes quite long from passing the send ...

Maciej by Associate II
  • 4627 Views
  • 6 replies
  • 1 kudos

Resolved! How to terminate unused RF pins

Hello,If I have a design where I am not using the RF pins, is there a recommended way to terminate them? Can you just ground them all?Thanks

AJ_1 by Associate III
  • 1308 Views
  • 1 replies
  • 1 kudos

BLE notifications from STM32WB to Android are truncated

I'm executing the P2P Server on an STM32WB.  I have a custom client that can be ported to different platforms.  When I build the client for Windows-11, message exchanges greater than 20 bytes work okay.  When I build and run on Android, the P2P respo...

HCohe.1 by Associate III
  • 1196 Views
  • 1 replies
  • 0 kudos

How can I activate plastic SIM on P-L496G-CELL02?

Hy, we struggle to get P-L496G-CELL02 up and running. We created a Cube IDE Software project and are able to send AT commands to BG96. Now we entered a plastic SIM from 1nce and try to connect. Unfortunately we can not select plastic SIM. There is a ...

_legacyfs_online_stmicro_images_0693W00000bjwgXQAQ.png _legacyfs_online_stmicro_images_0693W00000bjwemQAA.png _legacyfs_online_stmicro_images_0693W00000bjwinQAA.png
harald by Associate III
  • 5394 Views
  • 4 replies
  • 2 kudos

Resolved! Time Sensitive Networking (STN) on STM32WB

Hello everyone, do ST actually plan to support STN (Time Sensitive Networking) on their wireless products ? For industrial applications this would probably be an interesting alternative to Profibus if it is robust enough :) Greetings,Andreas 

AndreasC by Associate II
  • 1736 Views
  • 2 replies
  • 1 kudos