cancel
Showing results for 
Search instead for 
Did you mean: 

LoRaWAN FUOTA example SX1262DVK1DAS & NUCLEO-L476RG

Stm32_dev
Associate

Hi,

While building the example FUOTA code from icubelrwan software expansion. I am facing "No rule to make target error" attached the screenshot. 

Tried to build after including the path of the folder but still facing the same error. attached the screenshot.

Support me in resolving this error.

Thanks.

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @Stm32_dev and welcome to the Community :),

I apologize for my late reply.

Thank you for bringing this issue to our attention. I confirm the issue when using STM32CubeIDE 1.15.0 and I reported internally.

It is mentioned in the release note projects of I-CUBE-LRWAN that the development toolchain and compiler used for this package is STM32CubeIDE v1.6.1. For that please try to update the STM32CubeIDE toolchain.

KDJEM1_0-1715612609304.png

May these posts can help you: Post1 and Post2.

Internal ticket number: 181244 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hello @Stm32_dev and welcome to the Community :),

I apologize for my late reply.

Thank you for bringing this issue to our attention. I confirm the issue when using STM32CubeIDE 1.15.0 and I reported internally.

It is mentioned in the release note projects of I-CUBE-LRWAN that the development toolchain and compiler used for this package is STM32CubeIDE v1.6.1. For that please try to update the STM32CubeIDE toolchain.

KDJEM1_0-1715612609304.png

May these posts can help you: Post1 and Post2.

Internal ticket number: 181244 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.