STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

WB5M & OTA

Hello,I have developed a custom board around the WB5M and I am working on adding OTA support to it using the sample code from CubeWB -> Projects -> NUCLEO-WV15CC -> Applications -> BLE -> BLE_Ota.I have modified this code to use CMake (following the ...

STM32WL55CCU6, power drop requires reprogramming

Good day, We have a battery-operated device using the STM32WL55.The battery voltage is regulated to 3.6V as supply to the STM32.We have found when the battery runs flat, the STM32WL5 would often need to be reprogrammed. This doesn't happen when we pl...

TitanD_0-1728640558918.png
TitanD by Associate
  • 1109 Views
  • 1 replies
  • 0 kudos

Resolved! Target Unknown Error 32

 Yesterday evening I worked on an application for a Nucleo-WL55JC and STM32CubeIDE could connect to the ST-LINK just fine. I closed my PC and this morning started it again. I am trying to upload code to the CM0Plus core and now I am getting the follo...

Hvan .2 by Associate III
  • 6218 Views
  • 5 replies
  • 1 kudos

Resolved! STM32WB5MMG LSE clock 32.774 kHz?

Hello all,I want to use the STM32WB5MMG module for a project which requires an RTC.The datasheet states the module integrates a 32.774 kHz LSE crystal. That seems a bit strange to me because the standard clock for LSE is normally 32.768 kHz. Checking...

EricNava by Associate III
  • 2887 Views
  • 5 replies
  • 1 kudos

Resolved! How to configure STM32WB0 for HCI Controller Only mode

Hi there.I'm trying to use the STM32WB0 (NUCLEO-WB09KE) in HCI Controller mode with our Bluetooth Stack: https://github.com/bluekitchen/btstack/I found the BLE_Transparent application in the STM32WB0 Firmware package which provides HCI over the virtu...

mringwal by Associate II
  • 3106 Views
  • 6 replies
  • 0 kudos