STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55: Zigbee - Attribute Reporting

 Hi,I'm working on implementing attribute reporting on the Zigbee STM32WB55 Evaluation boards. I've attempted to configure attribute reporting in the Zigbee_DevTemp_Server_Coord and Zigbee_DevTemp_Client_Router baseline examples. However, I encounter...

BLE Always Fails when setting RFWKP Clock Mux to LSE

I've been having a lot of trouble getting all of the online BLE examples to work and was hoping someone could steer me in the right direction.  In every example they state that the RFWKP Clock Mux should be set to LSE but whenever I do that the main ...

nollstead by Associate III
  • 5865 Views
  • 12 replies
  • 0 kudos

Resolved! Dynamic Range of STM32WLE5 RF reciever

Hi , I see in the Datasheet in Table 31 some reciever parameters .I need to know what is the Dynamic Range of the Reciever in the STM32WLE5 . can you point me to which parameters should I look at ? Thank youViola

viola by Associate III
  • 1219 Views
  • 1 replies
  • 0 kudos

Resolved! Help needed with BLE server/client program

hi, I have two B-WB1M-WPAN1 cards and I would like to create a program that works as a client server, so one card will act as a server and then other client cards will send messages to it via BLE, I saw the example proposed by the company "BLE_HR_p2p...

snak3in by Associate III
  • 5892 Views
  • 13 replies
  • 2 kudos

Resolved! Merge library SubGHz and LoRaWAN on stm32wl5

Hello, I have a question regarding having both library (from the example files) SubGHz and LoRaWAN on the same microcontroller STM32WL5MOC at the same time and my idea is to use a switch to choose which on i would like to use depending in the case of...

User2501 by Associate II
  • 2295 Views
  • 5 replies
  • 3 kudos

Follow Up webinar on STM32WB0 MCUs

Hello,This message is for ST team.I attended the webinar on STM32WB0 MCUs, but I didn't receive the e-mail that was supposed to follow, including the links, recording and voucher for the demonstration board.What happens ?PS: I'm posting here because ...

Doom by Associate
  • 1522 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5 SubGhz Debug - Alternate functions

Hi , in the Datasheet there are few interfaces which are marked as "alternate functions" for DEBUG_RF or DEBUG_SUBGHZSPI.  ( Table 20 in the Datasheet)But , I didnt find any info regarding what can I use those function for ? for example - Can i acces...

viola by Associate III
  • 1977 Views
  • 5 replies
  • 1 kudos

Zigbee connection control

Hello, I have configured a Zigbee network using an STM32WB55 MCU with 1 coordinator device and 5 end devices. However, since I cannot check whether the Zigbee connection is lost or not, I am resetting the end devices every 1 minute using NVIC_SystemR...

oarslan by Associate II
  • 3372 Views
  • 10 replies
  • 0 kudos

Resolved! STM32WB55CG Zigbee LED Controller (Color)

Hi,I have used a custom board with an STM32WB55CG MCU to successfully connect to a Tuya Gateway and also a Homassistent/Zigbee2mqtt setup with the OnOff functionality.As next topic I wanted to add a color control functionility and tried several optin...

vh789 by Associate III
  • 4018 Views
  • 5 replies
  • 2 kudos