cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ASTRA1B low power

DS.4
Senior II

I see it has the WB55M and another WL module on it.

How is then the low power mode controlled?

Is it separate for each module?

Can I disable the other module? keep the WB55M only ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
STTwo-32
ST Employee

Hello @DS.4 

Each module is separated so you can control the low power of each alone and disable one of them to work only on the other.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

00shafiqahmad
Associate

Without more information on the specific device, it's difficult to say for sure. Here's what we can speculate:

Possible separate control: The WB55M and WL module might have independent low power modes.
Disabling the WL module: Disabling it might be possible, but proceed with caution. It could affect overall functionality depending on how the modules interact.