STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

B-WL5M-SUBG1 LoRa HAL Setup and/or TX Failing

Hello,I'm using the B-WL5M-SUB1G, using Visual Studio as my programming environment, attempting to get LoRa TX working without using the middleware.The code is below. The project serial output is below the code block. Referencing RM0453 Rev 6 (STM32W...

zbaltzer by Associate
  • 1115 Views
  • 1 replies
  • 0 kudos

Detect Zigbee Network Loss

Hi,I have the problem, that my MCU seems to loose its connection to the network quite often (after some minutes or hours usually) and is therefore not usuable.I would like to detect this in my Application and then trigger either a rejoin (if possible...

vh789 by Associate III
  • 1727 Views
  • 2 replies
  • 0 kudos

Resolved! UART not working with LoRaWAN

Hi, I'm using the LoRaWAN end node example from the stm32cubewl v1.3.0. The board im using is the RAK3172 based on the stm32wle5ccu6 chip. The application i want to build reads data from a modbus using UART and sends it through lorawan. I have assign...

KCB11 by Associate II
  • 2997 Views
  • 2 replies
  • 0 kudos

JSON Payload Not Received in Downlink in LoRaWAN

Hi everyone,I am using the LoRaWAN_AT_Slave example code on an STM32WL-based device, and I am operating in OTAA mode with the ChirpStack server to monitor the data. I am successfully sending sensor data to the server at the specified intervals.I have...

Downlink.png Downlink_Processing.png Downlink_JSON_Payload.png Downlink_Received.png

SPI setting speed is too low.

Hi, I'm testing a custom STM32WB09TEF7TR board. To communicate with the analog front end, I need to use SPI.However, SPI communication requires 17 us setting time, which means around 60 kHz.This speed is very slow.So, the Initiation of SPI becomes th...

scope_1.png
KKIM.6 by Senior II
  • 7551 Views
  • 3 replies
  • 0 kudos