STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WLE5 Shutdown consumes too much current

we are working on STM32WLE5 development.We succeeded to enter Shutdown mode and measured supply current of less then 40nA when operated at 3.0V,but at that time, the VDDRF and VDDPA were not connected (0 volts), meaning we could not test the LoraWan ...

aviad by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

Reading Zigbee window attributes does not work

I'm trying to get a window cover to work, but can't seem to get the communication between attributes to work. I've been able to do this with the on/off cluster but this just doesn't seem to work. Also the examples on github are programmed very differ...

Hesseltjuuh_0-1736943129961.png Hesseltjuuh_1-1736943136469.png

I2C on STM32WB09

I want to add I2C support to a BLE sample project, in particular BLE_Beacon or BLE_Peripheral_Lite.In CubeMX on non-BLE projects I can select PB6-PB7 for SCL-SDA respectively.In a BLE project there is a clash with TIMER and the I2C code is not genera...

LVanr.1 by Associate III
  • 1028 Views
  • 1 replies
  • 0 kudos

Resolved! LoRa FHSS Receiving in STM32WL55JC (E5) module?

I want to work with Lora FHSS. Resources on this subject are limited. \STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\SubGHz_Phy_LrFhss. ;I looked at the FHSS example you told me about. This example works in TX mode only. It on...

bozgan by Associate II
  • 2220 Views
  • 6 replies
  • 2 kudos

B-WL5M-SUBG1 Demonstartion Software Source Code

Hi there! I'm just starting with the B-WL5M-SUBG1 and would like the source code for the program that runs on a newly purchased development board. The documentation says this code is available https://www.st.com/resource/en/data_brief/b-wl5m-subg1.pd...

B-WL5M-SUBG1.png
davidn by Associate II
  • 1290 Views
  • 2 replies
  • 1 kudos

Resolved! LoRa FHSS support for STM32WL55JC (E5) module?

We purchased the STM32WL55JC Long Range Module board for a project. This board includes the LoRa E5 HF module. We are considering using LoRa FHSS in our project. Can this motherboard support LoRa FHSS? Does it support? I couldn't find much informatio...

bozgan by Associate II
  • 3083 Views
  • 6 replies
  • 4 kudos

Resolved! Doubts regarding timers

What are the differences between LPTIM and TIM, also doesTIM1,TIM2,TIM16,TIM17 work when the device is in STOP2 mode?

pho3nix by Associate III
  • 1285 Views
  • 1 replies
  • 0 kudos