STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to program STM32WB09KE in boot mode?

On page 39 of UM3345 (User manual - STM32WB09 Nucleo-64 board (MB1801 and MB2032)):Note: With the BLE_p2pserver demo programmed in the NUCLEO-WB09KE, the low‑power mode is enabled tooffer the best low‑power performances. Therefore, on STM32WB09KE, th...

MQi.1 by Senior II
  • 2677 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WBA52 ADC DMA

Hello,I'm having some trouble using adc with dma and HAL. I noticed that in function HAL_ADC_Start_DMA Length parameter is multiplied with 4. Shouldn't be 2 (16 bit data from adc)?File stm32wbaxx_hal_adc.c line 1760 (checked with versions 1.2.0, 1.4....

cvs_dk by Associate II
  • 1492 Views
  • 3 replies
  • 0 kudos

Resolved! RF transmit power on STM32WB with Zigbee stack

Hello,The datasheet for STM32WB55RG (DS11929, 3.6.1 RF front-end block diagram, page 22) states that the output power is user programmable:"In Transmit mode, the maximum output power is user selectable through the programmable LDO voltage of the powe...

0693W00000Bb3r6QAB.png
ABrua.1 by Associate II
  • 4850 Views
  • 6 replies
  • 0 kudos

Resolved! Pairing STM32WB55 with Windows with no IO capabilities

Hi, I am trying to pair STM32WB55 (slave) with windows (master) on a custom setup. While pairing, I am getting this error. The STM32WB55 must have no IO capabilities, and hence configured as No Input No Output. This seems to show that authentication ...

tmk_0-1738869328778.png tmk_1-1738869505198.png
tmk by Associate II
  • 1756 Views
  • 3 replies
  • 3 kudos

STM32WL55J sharing ADC and SWJ-DP

Hi,  For a project I need 12 ADCs. STM32WL55JCU6 has all the necessary ADCs but two of them are shared with SWDIO and SWCLK pins. Is there any good suggestion for being able to use both these functions at the same time?

Emendion by Associate
  • 2322 Views
  • 8 replies
  • 3 kudos

Resolved! STM32WL5x: Undocumented Bug in IRTIM Module

Hello,I have been developing a program on the NUCLEO-WL55JC1 development board, and I found a bug in the IRTIM module. The reference manual says that, when enabled, the IRTIM module will NAND the outputs of TIM16 and TIM17 and output the signal on a ...

AJ_1 by Associate III
  • 2844 Views
  • 4 replies
  • 4 kudos

Can’t get SWV to work on my NUCLEO-WL55JC1

Hello,Apologize for the long post/question…Using the NUCLEO-WL55JC1 board, I am trying to get SWV to redirect printf() output to the IDE console, with no luck.I added the below code to syscalls.c and modified the _write() function to call this functi...

MBaza.1 by Associate II
  • 1462 Views
  • 3 replies
  • 0 kudos