STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! NUCLEO-WB05KZ arduino IDE

Hello,Please i have question.for the board : NUCLEO-WB05KZ : Can I program this board with arduino IDE? If you have simple tutorial codes for BLE to get you started, please let me know.Thanks

ljm by Associate III
  • 2079 Views
  • 6 replies
  • 1 kudos

STM32WL33 Boot Loader and startup

Hello all.I'm writing an application using an STM32WL33 device, actually facing continuous problems related to the documentation and SDK, that seems to suffer (understandable) youth issues.After having solved many, I came now to several problem I can...

CZamb.2 by Associate II
  • 1207 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB55RCV6 RAM segments

Hi   If I understand correctly, this table in the datasheet says WB55RC family which I have a 256K flash type, should allow me to have 128K SRAM 64KB SRAM1 and 64KB SRAM 2 But the code that is generated with STM32CubeMX does not grant me all these s...

mahdiquestat_0-1739299493079.png

Resolved! STM32WPAN extern variable error

Hi, I am using a custom PCB with SM32WB5MM module. I am reading a temperature sensor and I want to update its value to the advertising package in "a_AdvData".For this I made a "shared_variable" in my main.c (for now its just defined to 10, later it w...

KlemenPfce_0-1739349093588.png

Resolved! B-WL5M-SUBG1 (MB1779B) and V3minie

Hi,i'm trying to work with Sigfox and MB1779B board.I try to connect with cube programmer and V3miniE.here is the log :is there a procedure to connect to board ?thank you

dam74_0-1739290535898.png
dam74 by Associate II
  • 3831 Views
  • 10 replies
  • 3 kudos

Help me to build a Zigbee project from scratch.

Hi, everyone. This is my first post.I want to build a completely new Zigbee project with my STM32WB55DK. I just want my device can connect to non-STM zigbee devices and STM zigbee devices and send my strings. Can someone teach me how to do it? The ex...