2021-07-06 05:49 AM
New to STM32WB.
I have 2 units of STM32WB5mm-dk boards. On these boards want to run BLE mesh code.
But when i checked in STM32WBCubeMX no BLE mesh example code for STM32WB5mm-dk.
Can some one help me in getting example code so that i can start development.
Generic onoff code would fine to start ?
2021-07-06 09:07 AM
Hello @RS.8akhare and welcome to the Community 🙂
You can have a look at the AN5292 and AN5289 How to build a wireless and Bluetooth Low Energy mesh application for STM32WB.
You can also start your application from CubeMX tool, for that please have a look at the attached document.
You'll probably get inspired from BLE Mesh examples within STM32CubeWB package: \Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\
You have also these resources:
Please mark my answer as best by clicking on the "Select as Best" button if it helped 🙂
If you still have issues, don't hesitate to come back to the Community and adding more details to your post.
Imen
2021-07-13 12:41 AM
Thanks for reply @Imen DAHMEN
I am going through the links and information you provided, all seems related to Nucleo board.
May be I have put my question in wrong way.
We have STM32WB5MM-DK discovery board. as you said I can see BLE Mesh lighting code under Nucleo board, but when I search same for STM32WB5MM-DK discovery board, there is no BLE mesh related code available.
So my question is, is it possible to port BLE mesh code from NUCLEO board to STM32WB5MM-DK discovery board in STMCubeIDE / Keil uV ?
If possible, what the changes need to be done so that I can run BLE mesh code on STM32WB5MM-Dk Discovery board.
Thanks !!
2021-07-13 05:18 AM
Hi @RS.8akhare ,
Is it possbile to port BLE mesh code to STM32WB5MM-DK discovery.
I recommend you this workshop: STM32WB Bluetooth Mesh Workshop, this will help you hrough hands-on exercises to develop Bluetooth Mesh using STM32WB5MM-DK board.
Imen
2021-07-13 06:26 AM
Hi @Imen DAHMEN
When click on "Access the Course" I don't see any material in it, below is screen shot. I have log-in credentials registered on STM.
Is there anything I am missing here ??