NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm trying to implement a DHT22 humidity/temperature sensor in the Lorawan stack. The stack works fine, as does the sensor, but separately. When I try to combine them so that each time I send the data, the sensor reads it, they don't work.
If I tried to connect Nucleo-WB55RG with CubeProgrammer GUI and CUI to update wireless stack using swd connection, the behavior of each was different.I could start FUS and update wireless stack on GUI, but cannot start FUS and update wireless stack l...
after looking over all the documentation i could find (datasheet, reference manual, etc.), i could not clearly find how i am meant to connect IR LED(s) for IrDA communication with an STM32WB55. The image i attached is a screenshot from the reference ...
Hello, I would like to know if the STM32 WLxx is supported by X-CUBE-STL. Because at this sitehttps://www.st.com/content/st_com/en/ecosystems/functionalsafety.html#functionalsafety-resourcesin the table below at the line RPN "X-CUBE-STL" the WL is pa...
I want to use HSE/1000 instead of LSE for the BLE Radio Sleep Timer Clock mux on the WBA6.Advertising works (being BLE peripheral), but after a connect, I immediately get a BLE disconnect (reason 8) when selecting the HSE/1000 input. HSEON bit is set...
Hello, I am developing a Zigbee SED application on the STM32WB5MMG in which I need to use the RTCs timestamps for logging. VBAT is connected to 3.3V and LSE is used. My expectation is, that the RTC keeps running while Zigbee Sleepy End Device is not ...
Hi ST community, I'm working on a project using an STM32WB55VGY, with the base code generated by STM32CubeMX v6.13.0 and HAL drivers v1.21.0. We aim to enable HSE and LSE Clock Security System (CSS) to detect clock failures and put the device into ...
The STM32CubeMX code generator allows you to enable the internal HSE and use it as the system clock source. However, when attempting to run the code, the system always fails into the Error Handler.
I am currently developing a board using the STM32WB09TEF7TR microcontroller.Unfortunately, when the device is powered on, the microcontroller does not function properly.It only starts working after manually resetting the reset pin.To diagnose this is...
Dear,I have a problem when runing this example code,fail to send all cmds if use directly uart1 port ,but can send successful cmd by using STLINK uart,i don't know why?Can somebody help me?both two ways i saw signal on GPIO23, but no response if dire...