STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TextArea with wildcard Array

Hi, I am currently working on a project to imitate a level display for an elevator. Using TouchGFX, i have 10 buttons with values 1-10 and once a button has been pressed it will add said value to a textbox with a wildcard on the screen. once that is ...

STM32U575 DMA2D - Synchronize framebuffer access

MCU: STM32U575VGTFT with embedded RAM: 16bpp, 8-bit 8080 interfaceI'm following this scheme in which the bramebuffer is transfered via DMA2D, as decribed in AN4943:As a comment, there is a limitation when transfering a rectangle with an odd number of...

ACC_0-1739288792910.png ACC_1-1739289457683.png
ACC by Associate II
  • 735 Views
  • 0 replies
  • 0 kudos

TouchGFX 4.20.0: Import of Custom Container

I wanted to import a custom container from another project. It however does not work because typographies and images are already present in the current project. I use the same buttons in several custom containers and screens. In this case it should b...

awiernie by Senior II
  • 2890 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFX Numberpad?

Is there a way to make the built-in TouchGFX keyboard act as a numberpad? I just want a way to enter numbers, decimals, backspace, and confirm data entry. This is for the STM32F469I-Disco board.