STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to use display ?

Hello everyone, I am newbie on stm32 (stm32373c-eval). I need help to use display. Can any one suggest me a link or full guide to use it.Thank you in advance....

Dkuma.13 by Associate II
  • 1416 Views
  • 1 replies
  • 0 kudos

Is it possible JPEG HW decoder output as RGB565?

Hi,I would like to change the example JPEG_DecodingFromFLASH_DMA to decode the JPEG file data to a frame buffer in RGB565 and then send this buffer to a 320x240 SPI TFT display. Only using the internal SRAM of the STM32H743VI. Is it possible?

Asantos by Senior
  • 1993 Views
  • 3 replies
  • 0 kudos

STM32F769I-Eval JPEG IMAGE capture using DCMI.

We are using STM32F769I-Eval for capturing IMAGE in jpeg format using DCMI. we are able to run In-built example of storing image in bmp format,bmp to jpeg image conversion.From our understanding,it is going through RGB565- ARGB888- RGB888 ,then bmp h...

Tp by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

When are invalidated areas re-rendered?

I am running an experiment to try to see how I can improve RENDER_TIME performance. In this experiment I have two items on the screen close to each other on the screen.One is a circle who's start and end angles are changed. The other item is a text ...

scottSD by Lead
  • 2694 Views
  • 5 replies
  • 0 kudos

Resolved! cubemx error

Use cubemx to generate touchgfx, open vs file compilation, error occurs

0690X000009ZYZNQA4.png
lxw by Senior
  • 1551 Views
  • 4 replies
  • 0 kudos