STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

OSWrappers & Keil RTX

Hii referee to this link and try to modified OSWrappers  for keil RTX5but all my efforts were in vain :sleepy_face: is it possible "touchgfx" provide true config for OSWrappers  & Keil RTX ?

Natali by Associate III
  • 1991 Views
  • 3 replies
  • 0 kudos

Resolved! external FLASH

HelloI use STM32F769I-DISCO board and STM32CubeIDE.The image is displayed correctly when the image is imported to the internal FLASH, but the display is distorted when trying to use the external FLASH.For details, the display will be distorted if the...

Ebun.1 by Senior
  • 2444 Views
  • 5 replies
  • 0 kudos

tutorial3 , Step2:Saving data

HelloRefers tohttps://touchgfx.zendesk.com/hc/en-us/articles/360018668232-Step-2-Saving-dataIn Screen1Presenter.hppmodel-> saveHour (hour);How do you get an instance of model?AlsoIn Screen1View.hpppresenter-> saveHour (hour);How do you get an instanc...

Ebun.1 by Senior
  • 787 Views
  • 3 replies
  • 0 kudos

Resolved! Why can't I access following help articles?

A few weeks ago I read the following article but now it is telling me "You're not authorized to access this this page". Anyone know If there's just technical difficulties with the website or do you have to have some special access?https://touchgfx.ze...

BSunw.1 by Associate III
  • 1598 Views
  • 2 replies
  • 0 kudos

Hi Martin, I have tried tried to create 2 projects with the new touchGFXgenerator, both compile without errors but when i download to the board, the graphic dont appear even though the download is successful.

Im using STM32F746 . i have the pixel format set the same in LTDC and TouchGFXgenerator, i have double checked the settings and recompiled the code several times, i wonder if i am missing something. any advice would be greatly received.thanking you i...

0690X00000BwBSBQA3.jpg
BO Re.1 by Associate II
  • 759 Views
  • 0 replies
  • 0 kudos