STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How can I get started with OV2640 camera module?

Hi!I have a STM32 F446RE Nucleo board and that bord have DCMI included.I wonder if I only need to connect the OV2640 camera module to the GPIO's of F446RE and then I'm done?Or do I need to write some more code?Where do I start?The only information I ...

0690X00000BwMFwQAN.png
DMårt by Lead
  • 4102 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX removed from Graphics Middleware in CubeMX?

Hello I cannot see an option to enable advance graphics in STM32CubeMX in order to use TouchGFX. (In order to see graphics windown in middleware.) In the new update log it was written that they no longer support TouchGFX and Stemwin. Is it the reason...

GunkutA by Senior
  • 1139 Views
  • 2 replies
  • 0 kudos

Resolved! Workflow for TouchGFX on STM32H7 devices

Dear all,I still haven't understood how the workflow should be for applications that use TouchGFX on STM32H7 devices. As far as I understood there is not graphic support at all since CubeMX5.5.0. On the other side I seems that I cannot import an STM3...

mkrug by Associate III
  • 1751 Views
  • 3 replies
  • 0 kudos

Resolved! Fonts appearance differed in the updated version

Hi!I encounter the issue with font appears differently in the old and new version of touchGFX.The font I use : Noto Sans Medium.In the old version (4.10) the Noto Sans Medium looks thin and tallAt the same time, typography name for Noto Sans Medium f...

0690X00000Bw5UVQAZ.png
WDAI.1 by Associate II
  • 2494 Views
  • 4 replies
  • 0 kudos