Skip to main content
lxw
Associate III
September 21, 2019
Solved

Translation TextArea with Wilcard

  • September 21, 2019
  • 4 replies
  • 1160 views

I have implemented a TextArea without wildcards to display fixed Chinese content. I have now created a TextArea with wildcards and want to dynamically display any Chinese content in the TextArea buffer. But so far all that has shown is "??? ". How to operate, thank you

This topic has been closed for replies.
Best answer by Martin KJELDSEN

Your range was defined using the actual, rendered glyphs - Try defining the unicode ranges instead . e.g. 0x0-0xe000. I'm unsure if the designer is able to take in ranges like that for anything bug ASCII - And I'm not too familiar with proper chinese unicode ranges.

But let's investigate:

�?? = (U+53C1)

贰 = (U+8CB3) 

壹 = (U+58F9)

If i define a range of 0x0-0xe000 my Font_FZYTK_TTF_20_4bpp.cpp is 10MB and it has the following:

// Unicode: [0x58F9, ]
 0x00, 0x00, 0x00, 0xFA, 0x01, 0x00, 0x00, 0x00, 0x00, 0x00, 0xFA, 0x01, 0x00, 0x00, 0xC1, 0xCC, 0xCC, 0xFE, 0xCC, 0xCC, 0x6C, 0x00, 0x00, 0x00, 0xFA, 0x01, 0x00, 0x00, 0x00, 0x11, 0x11, 0xFA, 0x11, 0x11, 0x00, 0x20, 0xDD, 0xDD, 0xDD, 0xDD, 0xDD, 0x03, 0x70, 0x03, 0x00, 0x00, 0x00, 0x00, 0x66, 0xF2, 0xCE, 0xCC, 0xCC, 0xCC, 0xCC, 0xDF, 0xF2, 0x07, 0x00, 0x00, 0x00, 0x00, 0xDE, 0xF1, 0xC7, 0xCC, 0xCC, 0xCC, 0x8C, 0x47, 0x00, 0x40, 0x01, 0x00, 0x00, 0x56, 0x00, 0x00, 0xF1, 0x7B, 0x77, 0x77, 0xDF, 0x00, 0x00, 0xF1, 0x4A, 0x44, 0x44, 0xDE, 0x00, 0x00, 0xF1, 0x07, 0x00, 0x00, 0xDE, 0x00, 0x00, 0xF1, 0xAD, 0xAA, 0xAA, 0xDF, 0x00, 0x00, 0xE1, 0x18, 0x11, 0x21, 0x9E, 0x00, 0x00, 0x00, 0x4B, 0x00, 0x90, 0x04, 0x00, 0x00, 0x00, 0xC6, 0x00, 0xA3, 0x00, 0x00, 0xC3, 0xCC, 0xEC, 0xCC, 0xDE, 0xCC, 0xCC,
 

The other two unicodes are present as well.

You've made a slight mistake in your code. The designer already set the buffer for you, so you do not need to do it again. Also, when you simply paste the rendered characters into code i'm not sure this will always go well.

Try using unicodes instead - This makes your application work for me =)

void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
		
 Unicode::UnicodeChar tmp[5] = { 0x53C1, 0x8CB3, 0x58F9, 0x0};
 Unicode::strncpy(textArea1Buffer, tmp, TEXTAREA1_SIZE);
 textArea1.resizeToCurrentText();
}

 (I added a call to resize to the current text, but you don't need that).

0690X00000ARZisQAH.png

/Martin

4 replies

Martin KJELDSEN
Principal III
September 23, 2019

99% of these cases you

  1. Haven't defined a wide enough wildcard range in your text tab so the fontconverter can generate pixel data for the unicodes you need
  2. Do not have the glyphs available in your font (while having 1. right)

Check your generated/fonts/src folder for Font_*.cpp files to see which unicodes were actually found + generated.

/Martin

lxw
lxwAuthor
Associate III
September 24, 2019

I created FZYAOTI as glyphs and defined wildcard range Chinese range 4e00-9fa5.And generated a larger font file.However, in VS, the manually entered string is identified as GBK2312 and filled in to buffer.Attached a project, you can have a look, thank you very much!