STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DCMI+LTDC+USB - Why Not Possible

I am very intrigued by the new STM32H7A and STM32H7B value line microcontrollers. I think these will be a great success for ST. However, I am dissapointed to discover that I cannot configure an STM32H7A3ZIT in an LQFP144 package to use a camera, a ...

MHenz by Associate III
  • 2667 Views
  • 5 replies
  • 0 kudos

Resolved! What could make a specific GPIO (PA12 and PA11) on STM32L073V8T6 work when configured as an Input but not work when configured as output?

I have a static LCD, a couple of other GPIOs configured as output and SWD which are all working fine. PA12 does not work when I configure it in output mode and i toggle the pin. I have tried using PA11 also with no success. The .ioc file of my projec...

oolor.1 by Associate II
  • 4783 Views
  • 6 replies
  • 0 kudos

STM32F746G-DISCO+TOUCHGFX+QSPI - Problem

Hello! Sorry for my bad English...I have board STM32F746-DISCO.I generated project with CUBEMX and TouchGFX Designer. It works very well - I can see background picture and buttons. Pictures are located in "ExtFlashSection".But today, while uploadi...

EEuge by Senior
  • 1078 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX getting deleted by virus scanner

Trend Micro thinks TouchGFX\4.13.0, is a virus. It then instantly deletes the TouchGFX.exe file. This is the second time it has happened. The Violation is flagging as 'Unauthorized File Encryption' I know you said software doesn't use any file encry...

0690X00000D8TkGQAV.png 0690X00000D8TjwQAF.png
DMeis.1 by Associate III
  • 1252 Views
  • 2 replies
  • 0 kudos

Resolved! Tutorial 1 Run target error

I bought a stm32H747I DISCO for using TouchGFX.Now I'm following steps of tutorial 1, but Run target is not working. I will attach Detatiled Log.Thank you.-----------------------------------------------------------------------------------------------...

Runing TouchGFX based code from STM32CubeIDE

I cannot seem to get an Application Template to run from STM32CubeIDE.Using the following versions of tools:TouchGFX 4.13.0STM32CubeIDE 1.2.0Windows 10Here are the steps that I follow:From within TouchGFX:1. File->New2. Select Application Template ST...

JHarding by Senior
  • 19609 Views
  • 35 replies
  • 0 kudos