User Activity

Hi Everyone,I am working on a project with TouchGFX. I'm working with STM32H743X MCU. Project have MT48LC4M32B model external SDRAM. I was have an issue with screen that corrupted image on it. You can see below some example at picture.In expectation,...
Hi Everyone,I am tryin to use video decoding that came with TouchGFX 4.18 version. I have a hardware with STM32H743. I can use video decoding with "Direct to Frame Buffer" stretagy buy it's creat some corruption in frame. Image just sliding little bi...
Hi Everyone,I want to do e flash loader device that can be load binary to mcu via Swdio pin. Is any one can give advice about this? Maybe stlink hardware can be use or any STM32-Disco board can be use I don't know. I just want to create something li...
Hi everyone,I am trying to create an external loader for my project by ST's "How to create an external QSPI loader MOOC" lesson. Actually lesson's github repository have microcontroller and quad spi flash configurations that I use.  I just change som...
Hi everyoneI am working on a project with STM32H750 chip. I use internal flash for run application. I want to use vga display. So for this, I disabled touch controller and configured LTDC for vga. I fixid the erros and load tha aplication in chip. Wh...
Kudos from