STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

getting bitmap ID from C++ code

Hello, I have user parameters in my device and every single parameter will have 5 image. Image will be choosen acorrding the working scenario. I want to store bitmap ID in my memory area so want to get bitmap ID from C++ code.Touchgfx generates "Bit...

Epamuk by Associate III
  • 1233 Views
  • 2 replies
  • 0 kudos

TouchGFX 4.13 does not have Keil Compiler?

Hello,I am using TouchGFX 4.10 but want to use the latest version i.e. 4.13. The issue I am facing in this version is that there is no Keil Compiler I.e. I can't edit the generated code in keil henceforth. Want to know if there is anything that I can...

STM32L4R7VI DCMI with large image resolution

Hi Community,I'm trying to get an image from a camera with a resolution of 752x480.In this case, the size (752 * 480) / 4 = 90240 exceeds the maximum DMA transfer length 65535.And I get a broken image: 1/4 of the image is duplicated.Original image:DM...

0690X00000AAPmdQAH.png 0690X00000AAPgGQAX.jpg
MMele by Associate
  • 2470 Views
  • 4 replies
  • 1 kudos

How to debug Touchgfx for custom Boards?

Hello everyone ,I am new to touchgfx. I have a custom board with STM32f769II controller ,SDRAM with 16bit data bus from Micron,QSPI flash and with 7inch TFT display (RGB888). I firstly try to configure only LTDC to display a image on LCD from flash i...

Resolved! Custom Swipe Control

Hello.....I want to know about the swiping .Basically i want to implement my own swipe for that i want to know at what place your handling the swipe control and how...i hope you will help me.I am currently working on STM32L4R9AI-eval.Thank you....

prathima by Associate II
  • 1592 Views
  • 3 replies
  • 0 kudos

Recipe for target 'flash' failed

I am getting the following code error. The program build successfully in the simulator but when I try 'Run Target' it fails.I use the following Build settings. And the detail log is below.Run Target Generate Done Generate Assets ...

0690X00000D8EBQQA3.png
DMeis.1 by Associate III
  • 2546 Views
  • 2 replies
  • 0 kudos