STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Set values of LTDC Timing for stm32f429ZI

HelloI have a TFT_LCD 5.7 inch. I want start up it with STM32F429Discovery but I have a problem according to the LCD datasheet I have to set Vsync (Front-Porch) = 4.5 TH (Hsync Period).But I can't give float numbers to the LTDC registers. LCD datash...

Somid.16 by Associate
  • 2036 Views
  • 2 replies
  • 1 kudos

Resolved! TouchController::sampleTouch

HelloI use STM32F769I-DISCO.Touch the screen to jump to the following functions.bool OTM8009TouchController :: sampleTouch (int32_t & x, int32_t & y){  / * USER CODE BEGIN OTM8009TouchController_sampleTouch * /  TS_StateTypeDef state;  BSP_TS_GetStat...

Ebun.1 by Senior
  • 2474 Views
  • 3 replies
  • 0 kudos

Embedded World 2020

Hello,ST announced, they will not attend to Emdedded world 2020. What about touchgfx guys? Will you participate the exhibition? if no, is there any person from touchgfx as a visitor. if yes, can we meet them at exhibition area to answer our questions...

MuratUnal by Associate II
  • 1402 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE and TouchGFX integration

I am having difficulty integrating STM32CubeIDE and TouchGFX to run on STM32F746GDiscovery. I have (I believe) all the SW loaded. I can run IAR EWARM, Atollic TrueSTUDIO, STM32CubeMX, STM32CubeIDE, TouchGFX. I have read and followed too many articles...

Resolved! Makefile Linking .o files

I'm trying to use a function from a .c file (that I am trying to add to my project) in another .cpp file (touchGFX project screen.cpp), I included the header file, but I get an "undefined reference" error. I have figured out that this is a linking er...

TLahr.1 by Associate III
  • 2472 Views
  • 2 replies
  • 0 kudos

Resolved! undefined reference to `cosf' `sinf'

Hello, I'm compiling a custom project with STM32M7 using TouchGFX library on it. Recently, when I started to play with more advance functions from TouchGFX I get this error during the linking process:.........../libtouchgfx-float-abi-hard.a(Math3D.o)...

SGold by Associate II
  • 3193 Views
  • 2 replies
  • 1 kudos