STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! setWideTextAction() not having desired effect

Hi,I try to use setWideTextAction() to wrap my long text into new lines as it goes over screen.However, setWideTextAction does not seem to do anything.What I have done:-disable Auto-size and set text area size within screen limits (to generate code b...

Tuoman by Senior II
  • 2512 Views
  • 5 replies
  • 1 kudos

Resolved! STM32F746G-DISCO

HeI'm sending the program.I want to display min_current from main.c after pressing the START button in AreaMin instead of the min given by ButtonADD_MIN and ButtonSUB_MIN buttonsgreetings

AD�?b by Senior
  • 2026 Views
  • 4 replies
  • 0 kudos

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all...

AGendrau by Associate
  • 1488 Views
  • 2 replies
  • 0 kudos

JPEG_Decode_DMA function never ends

Hello,Still developping on my STM32H753VT6 with touchGFX. Instead of loading images with touchGFX designer, I want to decode a JPEG image and then display it on my LCD screen.For the moment I've just checked the example for the STM32H750B-DK demo boa...

AJT141 by Associate III
  • 1151 Views
  • 0 replies
  • 0 kudos

Resolved! TouchGFX list items limited to 7. Howto extend?

I use on screen scrolllist and in base.hpp havetouchgfx::DrawableListItems<MenuItem, 7> scrollList1ListItems;Where number 7 i cant change and when menu have 8 or more lines app crash.I make more diagnostic and locate, that TouchGFX can show and scrol...

0693W000005BV9aQAG.png
MM..1 by Chief III
  • 2013 Views
  • 4 replies
  • 0 kudos

TouchGFX with the Hardware Button

Hi,I am new to the TouchGFX library and trying to make it work with the STM32F429-DISC1 board. The touch display is working fine and I don't see any issues with it. I am now trying to work around the Hardware Button to work with the TouchGFX library....

Azeem by Associate II
  • 7466 Views
  • 12 replies
  • 0 kudos

how i shoud double buffering in touchgfx

hi evryoneiam developing ui on stm32f429 microcontroller and i wanna use touchgfx for my software.i use 32MB external sdram and start address 0xc0000000 because my ui is complex.when i use single buffer strategy evrything is ok but for some widget li...

Hpott.1 by Associate
  • 1941 Views
  • 1 replies
  • 0 kudos