STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! A button beneath a solid container is touched ...

I met a strange "problem" with TGFX. Let's say, on one screen, it contains a few buttons and a container. the container is on top of the screen and invisible when the screen is initialized. The problem is when I set the container visible, I found but...

zzzzz by Senior
  • 1731 Views
  • 3 replies
  • 1 kudos

Dynamic Bitmap display in vertical screen

We are developing on a vertical screen.(Set in TouchGFX Designer's Config-> Display-> Display Orientation)Use TouchGFX's dynamic Bitmap to load RGB888 data (64x32) into the buffer.If you set the generated data to Image Widget, the image will be disto...

fuka_m by Associate II
  • 4458 Views
  • 4 replies
  • 1 kudos

touchGFX application template

Hi all,basically we wanted to test creating a GUI with touchGFX for our STM32F103 (320x240 LCD via memory interface).First problem: after downloading touchGFX 4.10 and creating a new project, we have only 1 application template for simulator. We see ...

Simulating a backend, threads with simulation?

Hey guys -I've got a development where I'm going to use the simulator and share the build with a team to get thoughts/usability input/etc. So, I'm going to want to simulate input into the GUI. The model is using FreeRTOS queues to do the messaging ...

Jazman by Associate III
  • 1158 Views
  • 1 replies
  • 1 kudos