2020-11-06 8:48 AM
Hello,
I'm wondering if there is a an alternative to TICK_INTERVAL_MS constant which is deprecated. It is said that handleTickEvent() function is called by the Application on the current screen with a frequency of Application::TICK_INTERVAL_MS.
For the moment I've changed the frequency at which handleTickEvent() is called with this code :
/**
* Has to be called from within the LCD IRQ rutine when the Back Porch Exit is reached.
*
* Has to be called from within the LCD IRQ rutine when the Back Porch Exit is reached.
*/
virtual void backPorchExited()
{
static int cnt = 0;
static int modulo = 2;
if(cnt%modulo ==0)
{
swapFrameBuffers();
tick();
}
cnt++;
}(Here i got the same LTDC frequency but the frequency display is divided by 2)
regards,
AJT
Solved! Go to Solution.
2020-11-09 9:19 PM
To do so, you have to modify the HAL_LTDC_LineEventCallback() function.
Basically you are preventing the TouchGFX framework to render a new frame every time the display has finished refreshing itself.
You do so by calling OSWrappers::signalVSync() only every x display refreshes.
Here is a sample code :
extern "C"
{
static volatile uint8_t renderNextFrameNb = 1;
void HAL_LTDC_LineEventCallback(LTDC_HandleTypeDef* hltdc)
{
if (LTDC->LIPCR == lcd_int_active_line)
{
//entering active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_porch_line);
if(renderNextFrameNb%x == 0)
{
HAL::getInstance()->vSync();
OSWrappers::signalVSync();
// Swap frame buffers immediately instead of waiting for the task to be scheduled in.
// Note: task will also swap when it wakes up, but that operation is guarded and will not have
// any effect if already swapped.
HAL::getInstance()->swapFrameBuffers();
GPIO::set(GPIO::VSYNC_FREQ);
}
}
else
{
//exiting active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_active_line);
if(renderNextFrameNb%x == 0)
{
GPIO::clear(GPIO::VSYNC_FREQ);
HAL::getInstance()->frontPorchEntered();
}
renderNextFrameNb++;
if(renderNextFrameNb > x)
{
renderNextFrameNb = 0;
}
}
}
}When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-11-08 8:53 PM
Hello,
I'm not sure I get your point. Why do you want to change the frequency at which handleTickEvent() is called ?
handleTickEvent() is called every "display tick" which refers to every time a Tearing Effect event sent from the display is received by the MCU. Usually this period is around 16 ms.
/Alexandre
2020-11-08 9:32 PM
Hello
I just want to change the frequency of the display so instead decreasing frequency of the LTDC screen that leads to display glitches (like screen flickering), I change how many time we call handTIckEvent function.
And I don't want to change all screens handletickevent functions so is there a proper way to do that or did I do the right thing ?
Regards,
Ajt
2020-11-09 9:19 PM
To do so, you have to modify the HAL_LTDC_LineEventCallback() function.
Basically you are preventing the TouchGFX framework to render a new frame every time the display has finished refreshing itself.
You do so by calling OSWrappers::signalVSync() only every x display refreshes.
Here is a sample code :
extern "C"
{
static volatile uint8_t renderNextFrameNb = 1;
void HAL_LTDC_LineEventCallback(LTDC_HandleTypeDef* hltdc)
{
if (LTDC->LIPCR == lcd_int_active_line)
{
//entering active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_porch_line);
if(renderNextFrameNb%x == 0)
{
HAL::getInstance()->vSync();
OSWrappers::signalVSync();
// Swap frame buffers immediately instead of waiting for the task to be scheduled in.
// Note: task will also swap when it wakes up, but that operation is guarded and will not have
// any effect if already swapped.
HAL::getInstance()->swapFrameBuffers();
GPIO::set(GPIO::VSYNC_FREQ);
}
}
else
{
//exiting active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_active_line);
if(renderNextFrameNb%x == 0)
{
GPIO::clear(GPIO::VSYNC_FREQ);
HAL::getInstance()->frontPorchEntered();
}
renderNextFrameNb++;
if(renderNextFrameNb > x)
{
renderNextFrameNb = 0;
}
}
}
}When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-11-10 1:13 AM
Looks like it is working !
Thank you !