STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Invalidated widgets flickering

We use TouchGfx with a STM32f769 on a custom board. There are many ui widgets like textarea, boxes and buttons. At first the display had a flicker problem. That was solved with just invalidating widgets that should update.Now the problem is that if a...

MVils.1 by Associate II
  • 3658 Views
  • 13 replies
  • 0 kudos

TFT LCD using by TouchGFX

Hello, STI have some problem for display drawing.I encounted error on simulator when compiling TouchGFX so, I excluded simulator to compile.(after exclusing simulator, I could compile)(using TouchGFX library : cortex_m7/gcc/libtouchgfx-float-abi-hard...

0693W000003PiW3QAK.png 0693W000003PiW8QAK.png 0693W000003PiWSQA0.png 0693W000003PiWhQAK.png
Phyo .1 by Associate II
  • 902 Views
  • 1 replies
  • 0 kudos

Resolved! Simulator not detecting Hardware button clicked

Hi,I have implemented a hardware button that changed the screen displayed.It works fine when using the hardware.I also want it to work with the simulator using the computer keyboard.I think it is what the "Choose button key" in TouchGFX is for (corre...

0693W000007DUTqQAO.png

Resolved! Keyboard example how to

Dear community members,I wanted to use keyboard API but yet haven't found any "how to" for using this API. I know that there is an example in designer, but the codes are really advanced. Even the API documents are not going to make it easy to use (at...

LCD setting value of STM32F746G

Thank you for helping.environment:Board: STM32F746G-DISCOTouchGFX Ver 4.15.0The setting code output by TouchGFX is as follows.It does not match the value on the LCD data sheet.Please tell me how to calculate.Thank you.static void MX_LTDC_Init (void){...

Ebun.1 by Senior
  • 1061 Views
  • 3 replies
  • 0 kudos

Decrease Display FPS

Hello,i'm running touchgf in my 720x720 18bit display. I need to decrease the fps because of the heavy rendering time. I know that to decrease the refresh rate i need to change the LTDC clock frequency. Now it is working with 25MHz (which should be a...

AMerc.4 by Senior
  • 4888 Views
  • 10 replies
  • 0 kudos