STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

LTDC color keying in L8 mode

I am using an STM32H7A3ZI and am seeing some unexpected behavior with the LTDC color keying in L8 mode.Setup:2-layer mode. Layer 1 (background) is fully opaqueLayer 2 (foreground) has CLUT configured such that pixel value 0xFF maps to RGB (0,0,0), th...

Remi.G by Associate II
  • 1694 Views
  • 0 replies
  • 1 kudos

Alguien sabe como se puede solucionar este error? Error: Cannot find the specified linker script. Check the linker settings in the build configuration.

Buen día amables compañeros. Me encuentro trabajando en un proyecto con la placa STM32F746G-DICO en el entorno de desarrollo STM32Cube IDE 1.5.1 y el genrador de graficos TouchGFX 4.16.0.Pero al momento de complar el proyecto se presentan 3 errores.1...

JSarm.1 by Associate
  • 2937 Views
  • 4 replies
  • 0 kudos

LTDC color and DE signal

Thank you for helping.MCU: STM32F769BIBoard: CustomI set up LTDC using TouchGFX and STM32CubeIDE.I thought that the RGB color signal would be output in synchronization with the DE signal.When checked with an oscilloscope, the color signal (for exampl...

Ebun.1 by Senior
  • 1479 Views
  • 1 replies
  • 0 kudos

Resolved! TouchGFX : FreeRTOS Queues for controlling LED from TouchGFX Button and Hardware Button to TouchGFX Text Area Update:

Hi,I am working on below setup:Software Tool Chain:STM32CubeMX 5.6.0STM32CubeIDE 1.3.0TouchGFX 4.13.0 DesignerApplication Template STM32F746G Discovery Kit v3.0.1I am trying to do send/receive messages with Message Queues.1) From TouchGFX Toggle Butt...

0693W000000WTJpQAO.png