cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with migrated project between 4.13 to 4.15

MM..1
Chief III

My result for use CubeIDE versions is strange. Every version have deep troubles.

One my project i handle over versions and end with TouchGFX 4.13 in CubeIDE 1.3.1 and MX 5.6.1, with perfectly working code.

Half year after i use second PC and install newer TouchGFX 4.15 CubeIDE 1.4.2 MX 6.0.1

import project to workspace, regenerate ioc code with update fw 4xx from 1.25.0 to 1.25.2 , open TouchGFX project upgraded. Building project OK. BUT.

When i load to board first code, all gui work without glitch.

New code create anim, fade and other gui glitches on gui changes.

Then i maybe dont found it, but when exist web page , where is writed all versions ERRATA for this complex system , i need this info.

And ofcourse PLS autors dont release new versions , when isnt well tested.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0