STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to add several include path to TouchGfx simulator

Hi,I cannot figure out how to add several include path to for the simulator.I can add 1 path to the TouchGFX\simulator\gcc\Makefile as follow:project_path := $(call qs,$(abspath $(call sq,$(makefile_path)../../..))) app_path := $(call qs,$(abspath $(...

Define img, box, text

Hi guys,I would like to know, if I can somehow in general define img in program and use it in function. For examplevoid Screen1View::function1(random_img){image img;img = random_img;img.setAlpha(0);img.Invalidate;}The same way with Box with border an...

mckrek7 by Associate
  • 778 Views
  • 0 replies
  • 0 kudos

How to move a dot along a specified path?

Hi,In my demo project I have to move a dot along a L-shaped path continuously i.e. start over from beginning once the dot reaches end of the path. I would appreciate if you could point me to an example that explains hot to achieve this.Thank you in a...

BGuth.1 by Senior
  • 3089 Views
  • 7 replies
  • 0 kudos

Resolved! TouchGFX ScrollWheel widget index does not match UI

I have noticed what might be a bug in the updateItemCallbackHandler() in my screen's ViewBase file where the itemIndex consistently moves ahead 1 index when I swipe up. /* Scroll Wheel Item Update response to swiping is generated by TouchGFX */ void ...

0693W000008yw5aQAA.png 0693W000008yw5fQAA.png
TLe.4 by Associate II
  • 3831 Views
  • 6 replies
  • 1 kudos

How to use TouchGFX without freeRTOS

Excuse me?I want to use TouchGFX without FreeRTOS.​I make STM32F769I_DISCO's project with TouchGFX Designer.Next, I open .ioc file and disable FreeRTOS. I run this project, but the dhisplay is blank.​I want to tell me how to use touchgfx without Free...

onosho by Associate II
  • 1256 Views
  • 2 replies
  • 0 kudos