2020-12-13 6:47 PM
Thank you for helping.
How much SDRAM capacity does TouchGFX actually consume?
Please tell me the unit in bytes.
environment
board: STM32F769I-DISCO
TouchGFX: Ver4.15.0
Solved! Go to Solution.
2020-12-14 4:34 AM
Hi Ebun.1,
If you are using the application template available from TouchGFX Designer for the STM32F769I-disco board, the SDRAM is only used to store framebuffers. For this board, one framebuffer is set at the address 0xC000000. In general the amount of memory used by a framebuffer is equal to: the width * height * color depth in bits / 8 bytes, so in this case : 800*480*16/8 = 768000 bytes
/Romain
2020-12-14 4:34 AM
Hi Ebun.1,
If you are using the application template available from TouchGFX Designer for the STM32F769I-disco board, the SDRAM is only used to store framebuffers. For this board, one framebuffer is set at the address 0xC000000. In general the amount of memory used by a framebuffer is equal to: the width * height * color depth in bits / 8 bytes, so in this case : 800*480*16/8 = 768000 bytes
/Romain
2020-12-14 2:28 PM
Hi, Romain Dieleman
Thank you for your response.
I understand.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.