2020-11-26 4:11 PM
I want to display a warning window when a single triggered from hardware.
It seems that if I want to achieve this effect in touchGFX, I need to add a model window to each interface. Can I add a global window to implement it elegantly?:face_without_mouth:
Solved! Go to Solution.
2020-11-28 10:14 PM
If you are triggering a warning from hardware, I assume you want to call this function from the Model.cpp file.
I've accomplished this by creating a BaseLayer custom container with all elements common to all screens (such as warning modals) having their code defined within. This BaseLayer is added to all screens. I register a pointer in Model.cpp to the current instance of the BaseLayer. Then when I need the modal, I (carefully) call the function directly from the Model to the BaseLayer. This BaseLayer pointer needs to be updated every time it is instantiated or destroyed (i.e. every screen change), and nullptr checks need to be done in Model.cpp before it is used otherwise you risk a hardfault.
Here's how to do it:
It's not really "elegant" insofar as it doesn't follow the MVP pattern. However, I tried following the MVP pattern and calling a modellistener function to alert the presenters to call a view method to call a BaseLayer method... it's way too much hassle. Breaking the "rules" and selectively using a global pointer from the model to the baselayer is much easier as long as it is used sparingly and carefully.
Hope this helps. I've heard rumors of "Template Screens" coming in future TGFX versions.
2020-11-28 10:14 PM
If you are triggering a warning from hardware, I assume you want to call this function from the Model.cpp file.
I've accomplished this by creating a BaseLayer custom container with all elements common to all screens (such as warning modals) having their code defined within. This BaseLayer is added to all screens. I register a pointer in Model.cpp to the current instance of the BaseLayer. Then when I need the modal, I (carefully) call the function directly from the Model to the BaseLayer. This BaseLayer pointer needs to be updated every time it is instantiated or destroyed (i.e. every screen change), and nullptr checks need to be done in Model.cpp before it is used otherwise you risk a hardfault.
Here's how to do it:
It's not really "elegant" insofar as it doesn't follow the MVP pattern. However, I tried following the MVP pattern and calling a modellistener function to alert the presenters to call a view method to call a BaseLayer method... it's way too much hassle. Breaking the "rules" and selectively using a global pointer from the model to the baselayer is much easier as long as it is used sparingly and carefully.
Hope this helps. I've heard rumors of "Template Screens" coming in future TGFX versions.
2020-12-14 3:36 PM
My solution to this problem is to use a "static" instance of the container I need to show on top of the current screen and put it into FrontendHeap class.
class FrontendHeap: public FrontendHeapBase {
pubilc:
...
ErrorsWindowTop errorsWindowTop;
}This way you have an instance of the container (global window) that's created with the application and you can access it from every view and put it on the top:
Container& root = FrontendApplication::getInstance()->getCurrentScreen()->getRootContainer();
root.add(FrontendHeap::getInstance().errorsWindowTop);
root.invalidate();The function for putting a Top containet looks like this:
bool Model::addTopContainer(Drawable& d) {
FrontendApplication* app = FrontendApplication::getInstance();
if (!app->getTransition()->isDone())
return false;
Container& root = app->getCurrentScreen()->getRootContainer();
if (root.contains(d))
return false;
d.resetParent();
root.add(d);
root.invalidate();
app->registerTimerWidget(&d);
return true;
}I've added a method to Drawable class to reset the parent as otherwise it messes up the hierarchy:
void Drawable::resetParent() {
parent = nullptr;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.