STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Octo/Quad SPI RAM advice on graphical board

Hello, To have a powerful graphical interface, you need a lot of RAM.Can we use external RAM in Quad / Octo SPI for this?The ST kits with screens often have flash in quad/octo SPI but the external RAM is always in parallel (except STM32L4R9I-EVAL).I ...

pcu by Associate II
  • 2538 Views
  • 5 replies
  • 0 kudos

CubeMX + STM32F429I-Disc1 + STemWin

Hello,I have been working on the graphics display on the STM32F429I-Disc1, but have been unsuccessful and facing errors so far.Here are my specifications :CubeMX 4.25.0IDE SW4STM32 from AC6Repository FW_F4 V1.23.0 Board STM32F429I-Disc1Purpose : crea...

Sue.Jay by Associate II
  • 2055 Views
  • 4 replies
  • 0 kudos

STM32F446 Jpeg HardFault when image is too wide

Hello,I'm using LibJpeg from CubeMX to decode a jpeg file from SD-card and display it on an ILI9341 display. I found out that decoding will work only, if I decode an vertical rotated picture (240x320). If I want to decode the same picture horizontall...

georga by Associate
  • 601 Views
  • 0 replies
  • 0 kudos