STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Build Error

Hello, I am working with TouchGFX Designer version 4.25.0 and STM32Cube IDE 1.13.2 .Since today my build process does not work anymore and I get errors that some of the .hpp files are not existent. error notificationsI did double check the "missing" ...

Screenshot 2025-07-30 114012.png
Alx237 by Associate II
  • 559 Views
  • 4 replies
  • 0 kudos

Resolved! update a TouchGFX textArea from a .c file

I am trying to update a textArea object from a .c file.I have been able to open the screen by creating a wrapper, the wrapper also handles the data to update.  The screen is called ResultsView.cpp and the textArea is called textAreaTap to open the sc...

FJB2069 by Senior
  • 565 Views
  • 1 replies
  • 0 kudos

Resolved! Example of a ClickListener?

How does this work with a ClickListener?I have a view with 10 custom containers. How can I tell the view when a custom container has been pressed and which one? Do you have a simple example?ThanksRegards, Roger

Roger.ch by Associate III
  • 3439 Views
  • 3 replies
  • 1 kudos

Feature request: Export base magic numbers

When building a Widget or Custom Container, could it be possible to define values that can be used in the base and inherited class?Things that are in the base constructor.Coordinates, colours, Bitmaps_id, ...Predefined coordinates in Designer for whe...

Marc_LM by Senior
  • 404 Views
  • 1 replies
  • 1 kudos

TouchGFX Simulator Black background

Hi, I have encountered a new problem. When I run the simulator of my program, the simulator has a black background. But all the buttons keep their functionality and I can navigate through my designed sheets. I have updated my computer to Windows 11 a...

Screenshot 2025-07-31 085505.png
Alx237 by Associate II
  • 334 Views
  • 1 replies
  • 0 kudos