2025-03-05 10:38 AM
I am evaluating the MP line of processors and want to use TouchGFX. The current version of TouchGFX is 4.25.0 put the MPU addon is 4.24.0 and won't install with 4.25.0.
Is an updated MPU addon coming out soon?
2025-03-06 2:48 AM
It is not currently planned to have an MPU addon for the latest versions of TouchGFX. To evaluate STM32MP1 and TouchGFX, it is indeed necessary to align the versions of TouchGFX and the MPU addon.
This version already allows the use of a large part of TouchGFX on the MP1.
2025-03-06 3:41 AM
Thanks for the reply. The current MPU addon is looking for TouchGFX v4.24.0. That version isn't available for download anymore. Only v4.24.1 and v4.24.1.
Is there a place where i can get 4.24.0 so the MPU addon will align with it
2025-03-06 5:26 AM
Hi ,
Please go at this page : https://www.st.com/en/embedded-software/x-cube-touchgfx.html
and select the version 4.24.0, you should be able to download it.
2025-03-06 7:11 AM
Thanks, got it! I do see support MP1. Will the new TouchGFX eventually have support for MP2? That is what we are evaluating for a new project.