User Activity

Good morning, I recently created a project using an STM32F469NI - disco (2Mb flash, 320 KB Sram) board. Firstly, I created a project with the board default configuration, add the peripherals and labeled some pins. Later, I added Touch GFX as a softwa...
Hi there,I am doing a DIY project based on an STM32F469 disco board. I am using Touch GFX Designer v4.24 and generating the code with it.  The thing is that when I import the project to CubeIDE software, it does not take it as a cproject because it d...
I was just uploading the code without having any issue and after the new update of Cube IDE it just does not recognise the ST-LINK of the Discovery board (STM32F469). I attach the images. I tried to reset the board but can do it via ST-LINK Utility. ...