STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Is it safe to terminate and restart the thread that calls touchgfx:: HAL::getInstance()->taskEntry() ?

The reason is we have noticed both the display and touchscreen freeze after 3 months in our test suite so since these aspects do not share hardware it looks like the RTOS thread has latched.I have performed a preliminary test to perform the thread te...

TouchGFX Documentation Search Bug

When browsing the TouchGFX online documentation, pressing Ctrl-K (or clicking on "Search") displays a popup window where the search term is entered, and a partial list of hits is displayed with a link at the bottom to "See all xx results":When the "S...

0693W00000F9w1tQAB.png 0693W00000F9w1yQAB.png
DSwea.1 by Associate III
  • 747 Views
  • 2 replies
  • 0 kudos

Wrong LCD clock on STM32F429I-DISC1 Board

When selecting the STM32F429I-DISC1 Board, STM32CubeMX (v6.3.0) sets the LCD clock to 25MHz which is way to high.The LCD clock for the display should be 6MHz which could be set manually in STMCubeMX configurator on Tab [Clock Configuration] as follo...

MMeie.2 by Associate II
  • 763 Views
  • 0 replies
  • 0 kudos

making screen templates

Hi, I want to make screen templates so that users can choose the screen they want and add the project. Is there any possible way to do it?

Ezgi by Senior
  • 956 Views
  • 1 replies
  • 0 kudos