cancel
Showing results for 
Search instead for 
Did you mean: 

I didt call touchgfx function in my boot project but it is still linked into .text section

JJ.Lin
Associate III

Hi,

I didt call touchgfx function in my boot project but it is still linked into .text section, do you know how to avoid link touchfgfx code in?

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
MM..1
Chief III

How optimize level you set? Why you have touchgfx in project where isnt used?

Thank you for your reply, I just add a Boot configuration in the project which used to have Debug and Release. They can be toggled by macro configuration. And the touchgfx functions are not called under boot configuration.But the touchgfx do exist in "Build Analysis".