STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! RAM and ROM usage

Thank you for helping.Please tell me the amount of RAM and ROM used by TouchGFX.The version is 4.16.1.Thank you.

Ebun.1 by Senior
  • 1758 Views
  • 2 replies
  • 0 kudos

Resolved! Painters with Alpha in 4.17> removed ?

I use in my code setAlpha , but now dont exist. Why?class PainterRGB565 : public AbstractPainterRGB565 { public: /** * Initializes a new instance of the PainterRGB565 class. * * @param color (Optional) the color, default is black....

MM..1 by Chief III
  • 1460 Views
  • 1 replies
  • 0 kudos

Resolved! 8 bpp color palette

Question is if TouchGFX framework supports 256 colors? How to tie together hardware CLUT settings and framework?Due to internal RAM size limitations, I want to halve the framebuffer size by reducing the color depth from 16 bpp to 8 bpp . I cannot use...

VLau by Associate III
  • 3431 Views
  • 5 replies
  • 0 kudos

while(state) get stuck for ever !!!

hi im driving ili9341 lcd with spi1 and w25q128 with spi2 with stm32f103c8t6.im loading some images from w25q128 to lcd via dma (peripheral to peripheral).i should check if the last image has been sent to lcd or not before putting other images . so ...

Preis.1 by Associate
  • 1205 Views
  • 1 replies
  • 0 kudos

Resolved! How to distinguish which custom container was clicked?

Hello, I have a custom container with clicklistener, and I add two of this in my screen.How to distinguish which custom container was clicked?void CustomContainer::boxClickHandler(const touchgfx::Box& b, const ClickEvent& evt){ if (ClickEvent::...

V.H by Senior
  • 1048 Views
  • 1 replies
  • 1 kudos