STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Modal Window Enhancement

I'm working on an application that requires user interaction to edit text and number fields using a alphanumeric keyboard, and also to make "menu" selections using the TGFX ScrollWheel.I've designed data display and entry screens with objects that co...

0693W00000JPxb2QAD.png 0693W00000JPxbbQAD.png
DSwea.1 by Associate III
  • 2733 Views
  • 4 replies
  • 0 kudos

How to set color keying and LTDC sync?

1. There is a description of Color Keying in 16p of the document Link, and I want to know how to use it. I couldn't find anything in CubeMX's LTDC Tab that could set up for that register.​2. Also, is there a way to know the LTDC sync method in 7p of ...

Resolved! commercial use

Hi all,I need to know if TouchGFX in binary from could be use in commercial product. The official site (https://www.touchgfx.com/get-touchgfx/) says:"It is a free tool for production and redistribution on STM32 microcontrollers"so, i think i can use ...

ECiav by Associate II
  • 2066 Views
  • 2 replies
  • 0 kudos

What could cause TouchGFX incorrect colors in display and incorrect colors in SDRAM frame buffer values?

I am currently trying to display color properly on an RGB panel with parallel interface. However, colors are not displaying properly and I currently do not know what else to troubleshoot. I am using STM32F769I eval board connected to the RGB panel.I ...

0693W00000KZxyUQAT.png 0693W00000KZxzSQAT.jpg 0693W00000KZxvdQAD.jpg
RMolins by Associate III
  • 4634 Views
  • 7 replies
  • 0 kudos

touchgfx SPI touch controller

Hi!I am using is resistive touch panel which is handled by XPT2046 (TSC2046), Touch controller controlled by SPI. I added xpt2046 library to my file. I configured SPI_HandleTypeDef to mine. And I added code as you see below. What else do I need to de...

Uusta.1 by Associate III
  • 1471 Views
  • 1 replies
  • 0 kudos

Where to define setAnimationEndedCallback for my scroolwheel I want to .getSelectedItem(); when the scroll wheel stop spinning but have had a hard time to define the callback

i do not want to "presenter -> changeWPM(itemIndex);" when spinning but after spinning have ended ...Please help or point me to the solutionclass Screen1View : public Screen1ViewBase{public:  Screen1View();  virtual ~Screen1View() {}  virtual void s...

hjh by Associate III
  • 1148 Views
  • 1 replies
  • 0 kudos

How does one override handleDragEvent(const DragEvent& event); method of a SwipeContainer thet is a member of a View object.

I have a MainView that has a member Swipe containter. class MainViewBase : public touchgfx::View<MainPresenter> { public: MainViewBase(); virtual ~MainViewBase() {} virtual void setupScreen();   protected: FrontendApplication& applica...

manto.1 by Senior
  • 1292 Views
  • 1 replies
  • 0 kudos