cancel
Showing results for 
Search instead for 
Did you mean: 

Comparison of rendering times between two kinds image -> (L8_RGB565 and L8_ARBG8888).

V.H
Senior

Hi,

The same size images, one uses format L8_RGB565 with background colour and the other uses format L8_ARGB88888 transparent background. Two images for screen transition and the L8_ARGB8888 is smoother than L8_RGB565.

Screen2 used L8_ARGB8888 image and add a black box but it's smoother than screen1 used only L8_RGB565 image. How the image render when encounter transparent pixels in the image, the same width and height between two images.

Is it faster to render the same image with a transparent background ?

0693W00000GWPI8QAP.png0693W00000GWPINQA5.png0693W00000GWPIwQAP.png0693W00000GWPImQAP.png

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0