STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

UTF-8?

Hi,A colleague need to send me strings via Uart.He asked me whether I work with UTF-8, and I was unable to find this information or how to configure it...(I know that at the end of the day to display it I'll have to convert to Unicode). Does anyone k...

BBlad.1 by Associate II
  • 4164 Views
  • 4 replies
  • 0 kudos

The STM32L4R9 Discovery kit it comes with a small round (390x390) DSI based display. I am trying to setup a standard rectangular DSI based display. All the example projects for STM32L4R9xx use a round display using GFXMMU look-up table ...

Since I don't have a round display, I don't need this lookup table to convert the bit locations, but there is no obvious way to not use it. How do you bypass this GFXMMU look-up table method and just send the raw image array to the DSI path? I am usi...

slime by Associate II
  • 2002 Views
  • 4 replies
  • 0 kudos

New Image add to project - Application crashed

Hello everybody,I added an image to my project at the top of the list in TouchGFXDesigner.Sorting is automatically done by touchgfx designer. After that, my application did't run on the target anymore. I'm confused because this is causing a crash of ...

Force LTR text orientation

Hi all,I am struggling how to force a LTR text direction from a certain point onwards. For example in the image the version is written backwards as the first text has a RTL direction. I saw that it exists a specific LTR Marker with a code U+200E but ...

0693W00000KboqfQAB.png
MKsen.1 by Associate II
  • 2187 Views
  • 2 replies
  • 0 kudos

TouchGFX: Trouble migrating from 4.16.1 to 4.17.0

I'm having some troubles migrating a project from 4.16.1 to 4.17.1.My board is NUCLEO-H743ZIWhen linking a project after migration i get some errors like:"undefined reference to `touchgfx::TextArea::setTypedText("This error come from some auto-genera...

Roberto C by Associate III
  • 1949 Views
  • 3 replies
  • 0 kudos

MIPI-DSI Amoled LCD

Hi,I am trying to drive 454*454 px amoled lcd with stm32l4r9 mcu and the image cannot be displayed properly. I am using the cubemx settings and the desired settings according to lcd datasheet. Any advise ? 

0693W00000KbvMNQAZ.png 0693W00000KbvMXQAZ.png
er3481 by Senior
  • 2412 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX 4.18.1 - generated file build error

I recently upgraded my project from 4.16.1 to 4.18.1. After integrating the designer files in to my project build environment, I am facing build error with a designer generated file. See attachment. Obviously I cannot modify the generated files to a...

0693W00000Kbkr5QAB.png
BGuth.1 by Senior
  • 1167 Views
  • 1 replies
  • 0 kudos