cancel
Showing results for 
Search instead for 
Did you mean: 

I used the STM32 F767 custom development board, using the TouchGFX to drive the RGB screen, but when the picture is displayed, noise point

luke gong
Associate II

0693W00000GYL67QAH.jpg0693W00000GYL62QAH.jpg

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
MM..1
Chief III

Seems you use 565 RGB and all images is convrted to this format with dithering, or you have an hw trouble...

luke gong
Associate II

Yes, the RGB565 used, but the button is generated by TouchGFX, and there is noise display separately.

Yes, the RGB565 used, but the button is generated by TouchGFX, and there is noise display separately.

Like

Reply

Select as Best

luke gong
Associate II

Currently, it is the transparency cause, which reduces transparency can be reduced, but it is impossible to remove it. I don't know how to deal with it.